I have been searching for several weeks for an IC that does the following:
- switches a voltage between a VHI and VLO
- provides independent control over the values of VHI and VLO (as in, by adjusting the power supply fed to the rails of the IC)
- after switching, settles to 0.1% in <500 ns
- synced to external TTL trigger pulse (freq/rep-rate = 100 Hz, duty-cycle = 1%)
- ( VHI = 8V, must be able to scan VLO between 0V and 5V. )
For (1) and (4), anything that puts out a square pulse would do: FET driver, IGBT, function generator, etc.
For (3), I've noticed that DAC IC's tend to have great settle times.
But that's not enough! I have yet to find an IC that satisfies (2). Every IC I've found so far puts out a pulse that is either ground-referenced (VLO = 0V) or floating. I need to be able to independently change the high-level and low-level of the pulse.
I've tried a MOSFET, which satisfies (2), but does not settle quickly enough. The requirements above seem pretty basic, so I imagine there must be an IC designed for this sort of thing, but I can't find one.
NOTE: I'm not trying to drive a resistive load. The application is to switch the voltage (with respect to ground) on a small piece of metal very quickly and precisely.