This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommendations for a Space Constrained Offline 25W Power Supply

Other Parts Discussed in Thread: UC3844, TPS92010, UCC28600

We have a product that we need to operate offline, 85 VAC to 265 VAC, with a possibility of 300 VAC as we have a customer who uses 277 VAC.

The product that has 4 voltage rails :

24 VDC , 500mA                = 12 Watts

15 VDC, 500mA                 =7.5 Watts

5 VDC 200mA                     = 1 Watt

3.3 VDC 200mA                = 660mW

Total Load Watts              =21 Watts

Assuming 84% efficiency = 25 Watts drawn by power supply

 

The original design was 12 watts loads assuming 15 Watts.

The Bulk High Voltage Capacitor was sized at 47µF 450V.

Moving to the 25 Watt had to increase the Bulk Capacitor to 80µF.

 

The original design used a 3844 current mode controller with a flyback operating in Discontinuous Conduction Mode .

The 3.3V, 15V and 24V Windings were stacked to share current to help with regulation, the 5V winding was on its own but referenced to the stacked 3.3V, 15V, and 24V winding.

 

The switching frequency was set at 130Khz.

The primary was design to be 268µH

 

The Transformer was custom designed, and is in a EF20 bobbin with 5 pins per side.

The high voltage side of the transformer has a split primary, a boot winding, and a shield connection.

The secondary had 5v, 5V_GND, 24V, 15V, 3.3V and 24\15\3.3V_GND

The 3.3V supply was monitored and regulated on.

 

The power supply did its job, but at full load was running a bit warmer that we liked.

The Transformer had about 2.1 Watts loss.

The mosfet was a bit toasty since it was not valley switched  DPAK package.

The primary Voltage clamp, Mosfet Protection had about 1 Watt loss

 

We have the product in a custom enclosure with very tight size constraints.

The power supply has 30mm ( w ) ,70mm ( L ), 20mm ( H ) of available space in the package.

 

Since we needed to move to 25 Watts I have no room for the larger high voltage bulk Capacitor.

 

To save space, and reduce some of the heating I thought it best to abandon the UC3844, and move to a part with Valley switching, and limiting features.

I came across the TPS92010 used for LED lighting. It’s a BCM converter.

I thought by ding a single stage PFC ( active rectification ) that we could obtain an isolated raw DC, somewhere around 28V on the Secondary side.

We would then use low voltage switchers, and or linear regulators to obtain the various voltage rails as described above.

 

Physical size, cost, and heat are very important..

 

Does TI have any recommendations for parts?

 

I don’t mind keeping the current custom transformer design, but I have no room for a larger high voltage bulk capacitor.

The single stage PFC is a thought but of course the secondary side regulation components will make things toasty too.

 

Is there a fixed frequency current mode valley switching offline controller TI can recommend?

Would it be better to do a 2 stage design using PFC as a replacement to the high voltage capacitor, then use the flyback to provide the secondary voltages?

  • I think the best place to start is in the UCC28600 product folder.
    This application fits perfectly within this device's intention.
    http://www.ti.com/product/ucc28600 

    This is our popular "Green Mode" controller for low power offline flyback design.
    -Quasiresonant switching for highest efficiency.
    -Switching frequency depends on line and load
    -Several operating modes for light load efficiency

    I believe this is the best way to approach it versus doing a PFC first or combined.
    For your power range the UCC28600 would be the norm.

    There are several reference designs similar to yours.
    About 1/2 way down in the product folder, click show more.

    For the basic power and operating range:
    http://www.ti.com/tool/pmp4820 
    85VAC-265VAC Input, 12V/3A Output Green-Mode Synchronous Flyback

    Then for some hints at higher input voltages:
    http://www.ti.com/tool/pmp5067
    100VDC-650VDC Input 12V 40W Isolated Flyback

    There is a calculator tool to design with.
    It's easy to use and provides the critical values.
    Software (1)
    UCC28600 Design Calculator (Rev. H) 
    (ZIP 260 KB )    631 views, 26 Jul 2012

    Design as if all the power is on the single highest voltage output. 24V
    Get all your powerstage and magnetic design.
    Then you can look at either tapping off that 24V winding for your 15V, or running all the other DC-DC's off the 24V.
    You can add the 15V tapoff easy to your transformer drawing.
    You save perhaps one DC-DC converter in the process.

    Depending on your loading and tolerances needed and transformer turns ratios, you might be able tap off all 3 other outputs.