I am using a TPS61025 for power management on a board that is draws a max of 20mA, and usually draws an average of 150µA.
The capacitor I am using on the output has an ESR of about 5E-3 at 600kHz.
Reading through the datasheet, I see that the chip "prefers" an ESR of > 30mOhm for stability.
I have a layout with a zero Ohm resistor leading right out of the output of the TPS61025, before the capacitor.
I have three questions:
- My prototype works now. Should I bother at all adding extra resistance to compensate for the lack of ESR?
- Would it work to put a series resistor in the position that is now 0 Ohm, or does it have to be between Vcc and the output capacitor? I would like to try to avoid a new layout.
- Would a resistor of 0.2 Ohm be too much? I investigated, and resistors of lower value were ten times as expensive, and I would like to keep costs down, if it does not affect performance.
Thanks for the help!