Hello,
I was looking at TLC5940 for 4 strings of LEDs with 6 LEDs in each string. If the forward voltage is 3.3V, total would be 19.8V for each string which is greater than the LED power supply voltage which is up to 17V according to the datasheet. Can you please explain why there is a limit of 17V, is it the max. power the chip can handle (17V and max. current of 120mA which is around 2W) which is the dissipation rating in page 5?
http://www.ti.com/lit/ds/symlink/tlc5940-ep.pdf
Thanks,
Madhu