This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I am trying to implement TPS7A4700RGWT and TPS7A3301RGWT linear regulators in to a new PSU design. I have prototyped both ICs with little success. I will talk specifically about the positive regulator from here on. My schematic is as follows:
http://snag.gy/cIeru.jpg
This should attain a +12V output. I built this circuit up as depicted, but the regulator provides no regulation. The output voltage tracks the input voltage (minus a few millivolts). I was concerned the layout I used was the problem so I deadbugged the circuit with a new chip, and exactly the same problem occurred. I replaced R1 and R2 with a 100K pot, the wiper connected to the FB pin. As I varied the potentiometer, the voltage output started at about 1.4V, climbed to ~2.5V then snapped to maximum voltage output - well before the potentiometer had finished rotation. I tried using the digital control pins to vary the output voltage which did in fact work - but my design calls for very clean +ve and -ve rails, the negative part does not have digital control lines. When I try and implement the negative regulator - it does regulate voltage but the output 'wobbles' ~+/-100mV slowly. Lowering the recommended resistor value helped this problem slightly but it did not cure it. Are there a bad batch of regulators out at the moment? What could I be doing wrong in implementing these devices? Any help is greatly appreciated
Thanks, Dan
This issue should be directed back to mravica at the diyAudio forum as this does not appear to be a TPS7A4701 problem. Request a Users Guide, or errata sheet, for your power supply that explains the options.
From the schematic at diyAudio, and your description of behavior, I can only guess that the TPS7A4701 SENSE/FB pin is not connected to the + output. Try shorting SJ9.
Also, short SJ10 in order to connect the NR capacitor to Gnd, this will allow for soft-start to reduce possibility of output voltage over-shoot at power-up.
Hi David,
Oh yes mea culpa, my mistake, i have used 4700, what should i changed in that design to work properly.
Thank you very much
Davorin
Good point on the difference between the two '00 vs '01.
I'm not seeing anywhere in the documentation at diyAudio (in the schematic, or on the pcb) a place to add R1 & R2.
The diyAudio web page clearly lists the " ... TPS7A4700 single voltage output ..." .
I'll guess that the schematic is not properly labeled (i.e. '01 should be '00) and circuit is intended for the '00 device only.