Hi,
I am charging a 3.7v 510mAh li-poly battery with a 6v - 600mA solar panel. The load connected to the battery draws a maximum current of 200mA.
Is it fine to connect both the charger and load at the same time to the battery terminal?
How can I make the system such that even if battery is charged but if solar panel is capable of driving the load then it will drive the load instead of the battery?
Thanks
Shahbaz