This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65930's current consumption when OMAP3515 in suspend-to-RAM mode

Other Parts Discussed in Thread: TPS65930, OMAP3515, TPS65950

Hi,

 

could you please give the min, typ and max TPS65930's current consumption when OMAP3515 in suspend-to-RAM mode?

Thanks.

  • Hi,

    Please post these on  the related forum. This forum is not for TPS65930 device. You can use - www.ti.com/omappowerforum

    For this question: We have some numbers for power consumption in the Data Manual. Current consumption for the system (with OMAP and PMIC) is very difficult to estimate as there would be some other resources on PMIC that can be supplying other than OMAP. It may vary from system to system.

    You can try to ask OMAP team if they have any numbers in this mode. I would assume that they would have some figures, however, those would be for TPS65950. Those may be used as estimates for TPS65930.

     

    Regards,

    Gandhar.