Hello.
I have used the tps51120 ic to get the 3.3v & 5V output i was able to get the regulated 3V & 5V output and thevoltage for driving MOSFETS. But i didn't get the outputs from VO1(Pin1) & VO2(Pin2). the MOSFET used in the circuit was FDS6982AS. I have attached the circuit for reference. The voltage input to the ic is (12V DC). Please suggest us a solution to correct our circuit and to get the outputs.
Thanks,
Parani.