This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24765

Other Parts Discussed in Thread: BQ24765EVM, BQ24765

Accumulators is not charged. Charger design is equal BQ24765EVM. Tests “CHARGE CURRENT AND AC CURRENT REGULATION (DPM)” and “CHARGER Voltage Regulation” (User’s Guide BQ24765EVM, p. 6,7) does not work correctly. SMBus works very well.  Charger’s profile: I=2048mA, V=12592mV. Active load: U=10V. Charger status is U=6.18V, I=0A. Reducing of active load voltage to charger voltage (6.2V) starts voltage regulation, but charge current not exceed 100mA. VREF=3.3V       ICREF=0.73V   ACIN=2.6V       ACOK=3.27V    ICOUT=3.29V        VDDP=5.98V.

Waveforms are in next pictures:

5342.BQ24765.pdf