Hello,
i've changed the title of post. My problem is with TPS62730DRYR rigth now. I powered TPS62730 3.3V and i got 3.2V on output. Here's my scheme: Vcc is input voltage and CCVCC is output voltage. 
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you post your schematic and operating conditions?
How is pin 5 connected? If it is low, you will see Vin on the output minus voltage drops in the system. Connect it high to enable the buck converter.
Hello,
i made mistake in my first post. I'm using TPS62730 not TPS62732. I already change it.
Pin 5 is connected to CC2541 chip. Right now it's not installed on board because i want to make sure that everything works. So the pin you are asking for is connected to low. I will try to see what will happen when i give high on pin 5.
Hi, problem still appears no matter if i connect pin 5 high or low, i still got input voltage on output..
Please post a scope capture of Vin, Vout, SW, and pin 5 at around 10 usec/div.