Hi, I have TPS61163A and I like to check with you if I'm using it correctly.
I have a boost that connects to a series of 10 backlight LEDs that I sink through IFB1.
Then I have another 2 LEDs that are parallel to each other (with 25 ohm ballast on each). I like to connect them directly to VBAT and sink them through IFB2.
Is this setup reasonable? Should I connect VIN pin to the output of the boost for the 10 series LEDs?
[EDIT: Added image of the relevant schematics]
Best regards
Valter