This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About matching of transmitter and receiver.

Guru 19495 points
Other Parts Discussed in Thread: BQ51025, BQ500215

Does TI's 10W receiver(bq51025) correspond to other 5W transmitter(Qi alliance)?

Is it non-recommend function?

Or, to begin with, does function not match?

Best regards,

Satoshi

  • Satoshi,

    Great question!

    The bq51025 is a Qi-compliant receiver (the EVM passed all certification requirements for v1.1). That means it will work, in 5W mode, with any Qi transmitter.
    The bq500215 is a Qi-compliant transmitter (the EVM passed all certification requirements for v1.1). That means it will work, in 5W mode, with any Qi receiver.

    When paired, the bq51025 and bq500215 can provide a full 10W solution.

    Regards,

    Dick