The bq24171 "blinks" the stat pin at 0.5Hz to indicate when a problem exists, but there are no on board diagnostics beyond that. Is there a checklist or test procedure documented somewhere that can be used to determine what condition is causing the fault? I'm working on building my own from various sections of the datasheet, but some of it is less than ideal to work off of.
Thanks