In reviewing the data sheet of the TPS54550 device it would appear the load current could go to 0 A with the regulation being within 0.1% with a Vin of 12V. Yet when I run SwitcherPro it doesn't allow me to set the load current to less than 100 mA. I have a circuit that the load current will be below 100 mA. Will the regulation follow the characteristics show in figure 31 or could it be worse below is a snapshot of the circuit
Look forward to e2e comments
Thanks
Dave Logan