Hi Team,
There is the following figure for latched output over-voltage fault protection.
Is there application note or configuration example for auto-recovery?
My customer would like to know it.
Best regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Peter-san,
I believe the auto-recovery configuration is possible when I set R2 more smaller in Figure26.
For example, R2=10kΩ etc.(10k[Ω] x 23[uA] = 0.23[V] < 1.25[V])
Is my understanding correct?
In addition, I would like to ask one more question.
My customer would also like to detect two types of OVP failure by OR-ing connection.
Is it possible to achieve this function as the following figure?
Best Regards,
Yaita
Hi Peter-san,
Thank you for your continuous support.
My customer also considers LM5045 for another project and needs auto-recovery output OVP scheme too.
Is there recommended figure(schematic) for the requirement?
I believe the figure is the same as LM5035C discussed above, but would like to confirm just in case.
Your support would be appreciated.
Best Regards,
Yaita / Japan