Other Parts Discussed in Thread: UCC28631, LM5021, LM5023
Hi, I'm using the UC28631D Chip in a design that converts 55V to 15V via a flyback transformer with a 2.67 turns ratio. I cannot change the transformer in my design. As such, when calculating the resistors used for the VSENSE pin, I get values that are outside of the recommended thevenin equivalent. What is the effect of using such a design? Alternatively, the datasheet states that Rp MUST be 3.9k; what is the effect of changing it's value closer to 2k? (This allows the resistors to have a thevenin equivalent closer to the recommended range).