Hello,
I'm sure that the IC boots as pulse skip mode while in the same state both light load condition
and "the input voltage is higher than the output voltage".
Is this IC able to operate when the input voltage is higher than the output voltage?
- If it is possible, what voltage (Vin - Vout) does it require?
- If it is impossible, what voltage (Vout - Vin) does it require?
Best Regards,
H.Fujikawa