Hi Chaps,
I have designed a flyback DC-DC converter with the UCC28700-Q1 recently. It all performs well apart from a problem that was noticed when the outputs were monitored at a reasonably big time scale on the oscilloscope (500us per division). There appears to be a 1.5-2kHz triangular/sawtooth wave on both of the outputs and feedback winding. This introduces further ripple voltage on the original output capacitor ripple voltage, which is undesirable, of course. Moreover, it brings into question the operation of the device as it leaves unanswered questions.
Graphs of the operation have been provided in the inserted file.
The IC seems to work on maximum frequency for about 10 cycles so it builds up the outputs then it decides to slow down and skip 8 valleys on average for about 3 to 4 cycles. Afterwards the process repeats. My question is why does it not fix itself at say 2 valleys skipped and 100kHz for a given set line and load conditions? Basically instead of running a marathon it sprints, then slows down and repeats, thus, creating the undesired 2kHz ripple on both outputs that is observed in Fig.1. in the attached file.
Thanks for the support in advance!