This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TPS54550

Other Parts Discussed in Thread: TPS54550, SWITCHERPRO

Hello.
My customer is currently in use TPS54550, I have gotten a question about this product .

So , I have a question about TPS54550.

<Question>

Q1:Does this device will be able to use the Switching Frequency at 500kHz?

Q2:And , do you why that can be used the case of a Yes?

Because…

Download the Switcher Pro, was to operate the TPS54550 under the following conditions ,

the setting of "Switching Frequency" had become a 500KHz (RT = OPEN).

Use of the data sheet p13 Fig8 ~ 11 "Switching Frequency" in 500KHz is assumed to NG , but in this software you receive so no problem .

< Condition >

VIN: 11.64V ~ 12.36V

VOUT: 1.375V

IOUT: 5.0A

Could you help us?

Best Regards,

Pokkun