This is the original Circuit from Ti Crypto Connected Launchpad.
I want to modify this circuit to PoE (with TPS23750):
Do i need the Capacitors C36 amd C38 ?
Is it ok to connect the Shield of RJ45 connector over 1MOhm/4700pF to GND or should i connect it to VSS of the TPS23750 ?
I use the PoE example PMP5592.
Thank you