Hello,
Am using LMZ12008 IC With En pin will be driven by MAX16009 voltage monitor open drain ic.
What is the Sink current for EN pin to driven low.Can this MAX16009 IC able to sink ?
Regards,
Prasanna G
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have attached my design, Where we connected MAX16009's output having sink current( 2mA)to LMZ12002 enable pin.
As i read from datasheet LMZ12002 it says it has internal pull-up resistor ,So when Vin comes LMZ12002 will be on if enable pin is not grounded(sinked).
My design needs to hold the EN pins of LMZ12002 to grounded by MAX16009 .
So my question is how much sink current needed to drive the enable pin of LMZ12002 "LOW".
Waiting for your feedback since my design is in crucial stage.
Regards,
Prasanna G
The EN sink current for the LMZ12002 is about 7uA
The EN sink current for the LMZ12003 is about 7uA
The EN sink current for the LMZ12008 is about 20uA