Hi
I'm Jun, Hardware engineer in South Korea.
I designed Power supply using part LM3485.
The Control Board is composed of the motor, MCU, UART...
See the Below Block diagram
My Operating Tempeature Spec is -40 ~ +70 degrees.
This Control Board operates normally at +25 degrees and +70 degrees.
But the Control Board faild at -40 degrees.
The condition is below table
1) Load current(at +6.3V) is 40mA at No operates Motor.
2) Load current(at +6.3V) is 40mA+200mA at operates Motor. The Motor current is 190 ~ 210mA.
The Motor does not operate always. Opearting time is 10 seconds and No operate time is 30 ~ 60 seconds.
Operating Procedure is
1) Turn on the power
2) Check the current concumption
3) Check RS422 communication with PC.
4) Set the command "Motor ON"
=> "Power Short " occur immediately and Dead LM3485 & DRV8832.
The Circuit of LM3485
The Circuit of DRV8832.
I replaced C10 10uF => 470uF and it tested but Control Board faild.
I need TI help.
Thank you