Hello,
According to Figure 1 of TPS3700-Q1, should I use "VIT+"-"Vhys" as VIT-(min) minimum detection under voltage?
If yes, the VIT-(min) is 384mV(min). ( VIT+(min) - Vhys(max) = 396mV - 12mV=384mV)
However, the VIT- is specified as 387mV.
Should we use 384mV for worst case of under voltage detection?
In the TPS3702-Q1, the VIT+(OV) and the VIT-(UV) is specified. Thus, I can use VIT-(UV)(min) as worst case.
I couldn't understand reason that the TPS3700-Q1 timing diagram is described by VIT+ for under voltage detection.
TPS3700-Q1 Timing Diagram.pptx
Best Regards,
Ryuji Asaka