Does this module protect itself against reverse input hookup?
I'm using it as 24 to 12V to drive a motor and 24Vinput is from external source to the board inside enclosure.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does this module protect itself against reverse input hookup?
I'm using it as 24 to 12V to drive a motor and 24Vinput is from external source to the board inside enclosure.
I'm curious, if the input of the LM14203H is at 13 to 14.2V for battery, would the output programmed for 12V, drop slightly?
I'm ok with lower output as long as it doesn't shut down or not not regulating.