This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am having an issue with a prototype design with the LM2776. I have followed the suggested layout and component suggestions, but when I look at the output without a load, the output is -1.2V and not -5V (VIN is 5V) . When I apply 3.3V to VIN my output is around -1V.
When I put a load on the output the voltage does decrease as it should with a load at around 150mA load.
Any help or suggestions would be greatly appreciated.
Hi Alex,
What kind of power supply is providing VIN? Can you take a look at VIN waveform with oscilloscope at start-up situation?
Regards,
Juha
I think there was a problem with the length of my traces to the capacitors (they are about 4mm away from the leads. I soldered the components right the package leads and everything is working perfectly
Thank you for the response,
Alex
Hi Juha,
I am having a problem just like Alex. However, the problem appears to be related to start-up timing. Could you help me understand what is causing this? Thanks in advance.
-Jacob
Schematic:
In the two oscilloscope traces below, Ch1 = EN pin, Ch2 = +5V supply, Ch3 = -5V output
When input power ramps up slowly it works fine:
When input power is applied more quickly the converter does not work correctly:
Here are traces of the C- terminal in the case of correct and incorrect operation. Channel is assignment is the same except for Ch1 which is now the C- terminal.
Working:
Not working:
Hi Jacob,
I took a look at your layout and there are a few things you could improve:
-Trace to GND pin is quite long and narrow. You should connect input and output capacitors with short and wide traces to VIN,VOUT and GND pins.( Like you have done with fly capacitor)
-Capacitors C110, C116 and C109 should be close to VIN pin.
You can refer datasheet, page 15 for layout example.
Regards,
Juha
Hi Juha,
Could you explain why the part does not work as I have shown it here? I found that soldering a 0.1uF capacitor directly across pins 1 and 2 (-5V output) makes it work correctly, but I did not see any explanation in the datasheet as to why this is. It says "Place C_OUT on the top layer (same layer as the LM2776) and as close to the VOUT and GND pins as possible." which is obviously good design practice (lower noise, etc.), but as you can see in my case, the part is able to work fine with the layout I shared as long as the supply voltage does not rise too fast. Why is the LM2776 so picky?
Hi Jacob,
The layout is important because of large switching currents and high switching frequency. A proper layout is more than a good design practice. It is something you must have if you want to have stable operation of the LM27762.
Regards,
Juha