This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65265 Dynamic Response Optimization on Load Transient

Other Parts Discussed in Thread: TPS65265

Hi, Team

A car infotainment customer Flyaudio is using TPS65265 in their project. The DCDC2 is output 3.3V for eMMC.

When system power up, the output current will change between 0 and 300mA rapidly. And it makes big spur on output voltage. The   Dynamic Response of Load Transient is slow. Could you advice how to optimize it?

Here is customer schematic:

Here is waveform:

CH1: Output voltage (AC coupled)

CH2: Wavefrom on LX2 (pin 11)

CH4: Output current

Thanks

Kevin