In the UC3842 datasheet, there are some questions on an application circuit.
What's the purpose of the D3 and C4? Why there two diode rectifier in the circuit?
What's the purpose of the R9?
Regards,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the UC3842 datasheet, there are some questions on an application circuit.
What's the purpose of the D3 and C4? Why there two diode rectifier in the circuit?
What's the purpose of the R9?
Regards,
Brian
Hi Brian, this circuit is not in our datasheet. It does appear in some of our competitors datasheets for their equivalent part. Considering that many of the part values don't have units it's hard to understand some parts of the circuit. In any case I don't understand the reasoning behind the part of the circuit you have highlighted being put in.
I recommend you ask the owners of the datasheet, or perhaps more useful would be to refer to the TI datasheet
which has a fully explained application and implementation section, section 9, with an example schematic.
Regards,
Billy
This circuit uses the bias winding to regulate the output voltage.
The 68 Ohm load on the bias ensures that the effects of leakage inductance of the winding are eliminated.
Since the power supply will not start up with a 68 Ohm load directly connected to the 56k bias resistor, the startup is isolated from the bias Vcc with the second diode.
You can also see that Vcc is divided down and applied to EA- input.
This is a low cost method of primary side regulation.