Hi
I've a build prototype for wireless charging based on BQ51050, where Ibulk is around 360mA (R14 = 670Ohm). Everything is OK, end of charge is detected, charge stopped at the end when my current reach the limit 10% of Ibulk, because my resistor Rterm is 2.4K.
Transmitter and receiver are OK and working well
For the production, battery is different and current Ibulk must be around 166mA : I just modify resistor value R14 = 1.74kOhm (as on schematic attach) to reach the current required
Charging is OK at 166mA, but when Ibat decrease, Ibat never stop, charger never stop : TX OFF conditions never detected and I don't understand why?
Do you have an idea of what can happen? is there specific value, current or voltage to check during charging to understand what happen?
Thanks for your help