This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We got a questions from customer about bq24610.
Could you help us?
[Question]
- According to datasheet, "The minimm precharge/termination current is clamped to be around 125mA with default 10mohm sensing resistor."
If they use current sense resistor is 20mohm, how much is the minimum precharge/termination current? Does the low charge current compartor be related? (Iterm min = Vlc / Rsr ?)
- If ISET2 is 0V, does the minimum precharge/termination current be disabled?
They consider to design termination current detection by external circuit. So they want the minimum termination current is disabled.
Best Regards,
tateo
Thank you for your reply.
They want to disable only termination current. Is there any way to disable termination current and enable safety timer?
They consider when Viset2 is 0V, Iterm become 0A. So they suppose to be able to disable only termination current.
Best Regards,
tateo
Hi, Sorry for rush, but could you give us your feedback by the end of this week?
Best Regards,
tateo
Tateo,
The minimum precharge is 1.25mV on SRP-SRN. For 20mohm resistor, this would be 62.5mA. I don't believe there is another way to remove termination without TTC to GND. You can use a higher sense resistor value, but that would cost efficiency.
Regards,
Steven