Other Parts Discussed in Thread: BQ25100, BQ25120,
Hi, I have used BQ25010RHLR and Li-ion battery (3.7~4.2V, 10400mAh).
BQ25010RHLR supports 100 or 500 mA USB charging. So the 500mA charge rate worked well, although it took quite a time to fully charge the battery.
Now, I have to work with a single cell (3.7~4.2V) Li-ion battery that has lower capacity; 2600mAh, 250mAh, and 80mAh.
I think using the 500mA charge rate with the 250mAh and 80mAh battery will cause problems.
So my questions are,
0) Can I use 100mAh charge rate with the 250mAh or 80mAh battery when using BQ25010RHLR and USB charger?
1) If not, is there an alternative IC products that I can use?