This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5005: How set Load current limit in LM5005

Part Number: LM5005


Hi,

I am using LM5005 for my power supply.

Input: 12V to 60V DC

Out Put: 10.5V DC @2.5A

My problem is, I am not getting load current. Out put current is very low. only one LED is ON.

How to set max 2.5A Load current.

Note: I am using LM5005 Eval Board Schematic and component. 

Regards,

Himansu