Application usingTPS25910 eFuse will supply 3.3V to EN pin and FLT pin (through 5K pull-up) with no voltage applied to VIN.
Is this acceptable? Will device be damaged or have excessive leakage.
Assumming this is OK, the data sheet mentions that FLT output becomes operational when VIn is above 1V. So could the FLT pin output the wrong state as VIN powers up (EN still = 3.3V)?