Hi all,
( TPS60502 is not recognized by the part number box in this forum but since it's a non-isolated DC/DC converter I suppose this is the correct place to post )
I want to use a TPS60502 charge pump regulator with 1.8V fixed output. My output current is very low, a few mA tops.
It's not clear to me from the datasheet what the requirement is for the minimum input voltage. It says Vin > 1.8V and Vin-Vout > 1V. If the latter is required then Vin should be greater than 2.8V
Thanks,
Paul
--