This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I received a question from my customer.
The Iq is 10mA when the TPS61071 is no-load running.
But the maximum Iq in the datasheet is 30μA
What is this reason? And is there any way to solve the this problem?
By the way, my customer wouldn`t like to use powresave-mode(TPS61070)
The condition is following.
- Vin : 1.5.V, Iout : 10mA Vout : 3.3V(setting 3.3V)