Hi all,
Can LM3445 meet below spec?
AC100V Input
MUST: Non isolated
MUST: Triac dim.
LED one string Vf 30 -- 40V, LED Curent 100mA,300mA, 600mA
Only up to 300mA ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Can LM3445 meet below spec?
AC100V Input
MUST: Non isolated
MUST: Triac dim.
LED one string Vf 30 -- 40V, LED Curent 100mA,300mA, 600mA
Only up to 300mA ?
Hello,
Should work fine at 600 mA. Power components are external to the device and the power level is not high enough to worry about gate drive issues.
Thanks,