This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65142: TFT - LCD power spec

Part Number: TPS65142
Other Parts Discussed in Thread: TPS65150, TPS65154

Hi all

Would you mind if we ask TPS65142 and TPS65150?

Our customer are looking for Multiple-Output Regulator which meets the following specifications;

<TFT - LCD power spec>
Vin : 3.3V
AVDD : 9.6V/14.2mA
VCOM : 3.9V(*)
VGH : 18.0V(*)
VGL : -6.0V(*)
* About these current value, now we are confirming.

So, TPS65142 and TPS65150 are suitable for above specifications?
(We guess that TPS65142 and TPS65150 are suitable above specification.)
Could you give us the your recommendation?

And then, is TPS65154 suiable compared with TPS65142 and TPS65150 also?

Kind regards,

Hirotaka Matsumoto