This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, this is a mini-project for my undergrad module. Most of the controllers i see are in TSSOP packages which my school lab is not equipped to handle, hence my need for a DIP package. My specs are: Vin = 36V to 48V (DC), Vout1 = 24V @ 1A, Vout2 = 12V at 1A, Vout3 = 5V at 0.1A.