Other Parts Discussed in Thread: LM3409, LM3450, LM3447
I need a solution to change LED brightness according to the phase-cut AC line, from 0 to 100%. LED requirements are 12VDCmax and 2A max. AC line is 85VAC to 265VAC.
Will the LM3445 demo board (230VAC, 6W- 15W Isolated Flyback LED Driver) be able to achieve this (although it is rated only 15Wmax)?
Will the LM3450A eval board achieve it?
Do LM3445 and LM3450A need LM3409 for the dimming capability?
In other words, without LM3409, does LM3445 or LM3450A give constant DC voltage and current whether the AC input is phase-cut or not?
Beside LM3445, LM3450A, are there any other parts for this goal?