Other Parts Discussed in Thread: LM25061, TINA-TI, TPS24701
Dear All,
I have an application where I need to limit the rms value to the load to 0.8A @5V.
I wonder if an hot-swap controller as for instance the TPS24710 could be used for this kind of application, using the timer pin to allow an over-current for a certain amount of time.
Maybe it will not be exactly tuned on the rms current, since the equilibrium is reached when the time in which the current is greater than the imposed current limit is equal to the time in which the current is lower: T(I>I_lim) = T(I<I_lim).
Do you know some other method to get a rms current limiter (able to react faster than a fuse, let say some millisecond and with a good accuracy (5%))?
Thank you in advance.