Other Parts Discussed in Thread: UCC28730
Dear All,
one of my customer made PCB as per TI design#PMP40025, below are the steps followed and observations made, kindly need your valuable inputs.
1)They externally supplied the controller UCC28730 to observe the switching pulses, But not observed.
2) Supplied UCC28730 from DC bus but no pulses can be observed, But there is fluctuation in VDD voltage after 21V which is the turn on thresold voltage.
This is the initiation controller and I have to ensure whether its working and application in the circuit clearly.
They started Testing twice and observed spark each time, following are observations,
1) Increased AC voltage input through Auto transformer.
2) First time - MOSFET gone when AC input was gradually increased.
3) Second time: When AC input of about 98 V ac reached, there is a spark, Resistance R8, R11 & R12 are burnt, and transistor Q4 is short.
4) We suspected high current flow.
5) R11 & R12 are 0.5 ohm 0.5W each, R8 is 1kohm.
Also update if any info about turns or winding inductance of primary, secondary & Auxiliary is available with you
Rgds,
Aravind.