Other Parts Discussed in Thread: MSP430F5528,
We are experiencing an issue where our devices will occasionally have a higher current draw (between .5 and 1.5 mA when normally 70 uA) after the voltage drops below ~2V, and then is brought back up again. I first observed the issue when about half of the devices battery life were drastically reduced after the batteries were discharged once.
Our design uses the MSP430F5528 along with the TPS65721 for charging the battery and regulating the voltage. I tried reproducing the issue by connecting to a power supply while observing the total board current draw, and adjusting the voltage below 2 volts and then back up to 4. About 50% of the time, there would be this sudden jump in current, but the device appears to still operate normally. The only way to get the current back down is to remove power, resetting the MCU alone does not help. While I am not sure if the TPS is the source of this current draw, I am wondering if there are any conditions where a discharged battery could cause it to enter a mode where it is drawing constant current. And if so, is there any register settings or reset commands I could send to the TPS to prevent it?