This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5007: Input Range of Regulator for 3.3V

Part Number: LM5007


Can we use this regulator for following requirement.

vin = 20 - 32 VDC

Nominal Vin = 28V

Vout = 3.3V 

Iout = 0.150

Input supply could vary b/w 20 - 32V

operating temp = -40 to +85deg

and o/p current requirement also may vary b/w 0.100A to 0.150A.

Please confirm about the selection of part is right or not