This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support!
our project PMU is based on LM5116. The input voltage is 50V, and the output voltage is 24V. The output voltage is used for driver 2 motors ,and per motor power is 75W.
But when driver the motor, the start time up to 1.36S, the time is too long for our application. We do a comparative test that the DC power supplys the power energy for motors,and the start time is 0.2S.
We need 24V, and want to decrease the motor start time. So what is different for the test? And what can we do to decrease the start time?
Thank you !