Hello,
My customer as the following requirements, the device runs on C type battery (3.6V) and the behavior of the system is most of the time is sleeps and consumes 50 uA.
Once on every few minutes the system is awakened and consumed in the area of 100 mA and goes back to sleep.
Please advise me if TPS63051 is suitable for this application?
Vin=2.5-3.6V ; Vout=3.3V
Please keep in mind that the battery can go down to 2.5V and still provide the 50 uA in sleep mode.
Thanks in advance and regards,
Shai Berman