Hi,
I would like to use the BQ24650 to charge a 6V Lead-Acid Battery.
To test it, I use a 6V/4.5Ah battery and a Laboratory Power Supply instead a solar panel.
In my case, the solar panel would be small without a lot of energy...
In accordance with SLVA437A, I chose following values:
Vbulk = 7.5V
Vrech = 7.2V
Vin = 12V
Vmpps = ~18V
Lo = 15uH, Co = 10uF, Rs = 40mohm
RT = 390K
RB = 180K
RP-B = 1M2
When I connect my power supply the LED1 (STAT1) blink like it doesn’t detect the battery. The battery voltage moved between 5.7V and 8.2V with a duty cycle of 10%.
The TS voltage is around 2V,the MPPSET voltage is 1.33V and Vref is 3.4V.
Please find my schematic.
Best reCharger_V105.pdfgards,