Hi,
I've just used the simulator and realized now the circuit. But I am facing some issues.
webench.ti.com/.../webench5.cgi
In the simulation I can run all simulations quiet well, except the startup. There the output voltage does not reach the requested 95V.
Furthermore in the real circuit we can't reach the real output current. So the voltage never reaches 95 V if the load is 1.16 kOhm (= 7.78Watt). It stays at 75 mA for 1kOhm (5,9Watt).
So I can't reach the simulated output current. If I increase the input current the TPS goes into overcurrent protection and switches off.
Is there a reason for this behavior?
Best regards,
Constantin