Other Parts Discussed in Thread: TAS5132
Hi,
I confirm the operation of TPS54302.
I want to ask two questions.
(1) Rush current is generated when the current at startup is measured.
Is overcurrent limitation functioning even at startup? Some devices I used previously do not detect overcurrent at startup.
(2) TPS54302 is supplying VDD of TAS5132.
There is a filter in VDD, but does this filter affect the operation of TPS54302?
The bulk capacitor C36 in the attached figure uses two 4.7 uF OS capacitors.
Best Regards,