I have problem with the stress test of TPS54232D.
Vin is 15V, Vout is 12V.
For stress test when I connect a light load 10Ohms at the output, current consumption is 600mA and output voltage drops to 8V. But in datasheet it is written that it can handle upto 2A current.