Hi Sir
My customer is interested in TPS92661 function but they have question about is there any concern in driving 1A load
From datasheet, the load current could up to 2A ,my customer's concern is since the package is small and cause the distance between pin and pin is also small, they are curious that is the width of layout path enough for 1A load or is there any suggestion in such load current. In TPS92661 EVB, the load current is only 135mA and the width is around 0.5mm.(as I know , the width of 1A is around 1mm)