Hi team,
I can't understand input current vs input voltage characteristic that is TL750's typical characteristic. In datasheet, we can find below figure:
I have 3 questions:
1, If input voltage is below than min voltage, What will happen to the output?
2, When input voltage is below than min voltage, why the input current increase as input voltage increase?
3, If Io=0A, that is to say, it has no load. What are the input voltage vs input current curve?
Now, I use 50ohm resistor to serial with TL750's input, and the power supply is 12V. I find the TL750's input voltage is only 4V, and the resistor's voltage is 8V. TL750 can't work normally.
I know I can decrease the resistance to avoid this situation.
But I want to know the reason of this phenomenon. After all, other P2P LDO havn't this problem.
Thank you.